Technical FAQs

Ask a Question

Can a remote keypad cable be obtained that is longer than the 3 meter cable that comes with the ATV28 VW3A28101 kit?

No. The 3-meter one that comes with the kit is the only length available.

To obtain anything longer than this would require the customers to create their own cable.


CTA-ID : 2013585
Was this helpful?
What can we do to improve the information ?