Technical FAQs

Ask a Question

What is the part number for the HP cable that is required to use a PDA (h5400, h3900 or h3800) to connect to Power Suite?

Powersuite no longer supports pocket PC connection. The parts are not available.

It is required that the handheld product be able to communicate through a DB9 serial port using RS-232. This signal is converted by the Powersuite cable kit into RS-485 to connect to the appropriate drive or soft starter.
As of 10/2003 the current part number is 250178-B21. This is not a Square D part. It is by HP. It is not available from Square D.

CTA-ID : 2013356
Was this helpful?
What can we do to improve the information ?