Technical FAQs

Ask a Question

What are Dimensions for an ATV66C19N4?

H=38.6`` (980mm), W=23`` (583mm), D=14.76`` (375mm) . These dimensions would also apply for an ATV66C10N4, ATV66C13N4, ATV66C15N4.

The weight is 300lbs (136kg) for all except ...C10N4 which is 280lbs (127kg)


CTA-ID : 2013315
Was this helpful?
What can we do to improve the information ?