Technical FAQs

Ask a Question

What are the dimensions and weight of the ATV28HU90M2U, ATV28HD12M2U, ATV28HU90N4U, ATV28HD12N4U, ATV28HU90S6XU, ATV28HD12S6XU Altivar 28 drives?

The entire width of the unit is a = 8 in (200 mm), the entire height of unit is b = 10.8 in (270 mm), the entire depth of the unit is c = 6.8 in (170 mm), and the weight is 13.5 lb (6.1 kg).

This information can be found in ALTIVAR 28 Adjustable Speed Drive Controllers User`s Guide (Trilingual), Document Number: VVDED399062US.

CTA-ID : 2012997
Was this helpful?
What can we do to improve the information ?