Technical FAQs

Ask a Question

Can the Class 8502 & Class 8536 Type S devices be used on 50 hertz applications?

There are no issues assuming the devices selected are sized according to the selection criteria listed on Page 14-20 of Digest 173 and the control voltage code specified is rated for 50 hertz applications.

Note: NEMA size 7 devices are not suitable for use on 50-hertz applications.



CTA-ID : 2012829
Was this helpful?
What can we do to improve the information ?