Technical FAQs

Ask a Question

Can the Full Voltage Type 8940 pump panels be used on a 575/600 volt a.c. power systems?

These devices are UL Listed and marked ``Suitable Only For Use As Service Equipment`` at their respective voltages of 240 or 480 vac, three-phase.

CTA-ID : 2012810
Was this helpful?
What can we do to improve the information ?