Technical FAQs

Ask a Question

Which wire color corresponds to the connection for the 0v signal on the RJ45 side of the ATV28 unit connection at the port on the drive?

The color may not always be consistent so can not verify the color used for each terminal.
As a standard for the RJ45 connector, with the tab is turned down facing the device being plugged into, pin # 1 is on the left and pin # 8 is on the far right.

CTA-ID : 2013788
Was this helpful?
What can we do to improve the information ?