Technical FAQs

Ask a Question

Is the normally closed (NC) contact replaceable in the 9065 Motor Logic or Motor Logic Plus overload relay?

It is not.


CTA-ID : 2013782
Was this helpful?
What can we do to improve the information ?