Technical FAQs

Ask a Question

Is the thermal grease that is required when replacing an IGBT block on an ATV66 included with the IGBT kit?

No. Would need to provide Thermalloy Thermalcote II, Part No. 349 grease or equivalent.


CTA-ID : 2012914
Was this helpful?
What can we do to improve the information ?