Technical FAQs

Ask a Question

Can the FLEX58 Chassis Drive be installed in a type 4X enclosure.

No. FLEX drives cannot be installed in a type 4X enclosure since the heatsink and its  components will stick out the back of the enclosure and be exposed to the local environment.

NOTE: Please refer to the documentation associated with the product for further information, cautions or warnings that may apply to this issue.

CTA-ID : 2012900
Was this helpful?
What can we do to improve the information ?