Technical FAQs

Ask a Question

What is the Nema and IEC rating for the 9007ML limit switches<br />

The nema rating is 1,2,4,6,6P,12,13, and IEC rating is IP67


CTA-ID : 2013555
Was this helpful?
What can we do to improve the information ?