Technical FAQs

Ask a Question

When using a remote mount VW3A28101 keypad to control an ATV28 drive can the reverse function be disabled?

No, the reverse button cannot be disabled when using keypad command (LCC set to yes) with the remote keypad for the Altivar 28.
This drive does not have a reverse inhibit.


CTA-ID : 2013130
Was this helpful?
What can we do to improve the information ?