Technical FAQs

Ask a Question

What is the part number for touch-up paint on the 8839 enclosed Altivar ATV66.

RAL 7032 (Beige) is the standard paint.

If customer has Mod Q303 which reqeust different paint color the enclosure paint is ANSI # 49 (gray paint).
If customer has Mod Q304 the enclosure paint color is  ANSI #61 (light gray).

Contact Seneca for ordering.


CTA-ID : 7070
Was this helpful?
What can we do to improve the information ?