Technical FAQs

Ask a Question

What are the mounting clearances for the 8839 58M units? Can they be mounted side by side?

For the wall mount units, provide at least 3 in. of mounting clearance on each side of the drive and at least 6 in. of mounting clearance at the top and bottom of the drive.

Floor mount units may be mounted side by side without clearance. Provide at least 36 in. of mounting clearance in front of the drive and at least 24 in. of mounting clearance at the top of the drive.


CTA-ID : 2013533
Was this helpful?
What can we do to improve the information ?