Technical FAQs

Ask a Question

Can subfeed lugs be used on a SC2040M200S CSED device?

Yes. For subfeed lug applications up to 125 ampere maximum, use HOML2125.



CTA-ID : 2012285
Was this helpful?
What can we do to improve the information ?