Technical FAQs

Ask a Question

Does Schneider Electric / Square D offer any 200 amp main breaker load centers with feed thru lugs in a NEMA 1 (indoor) enclosure?

Issue:
Load centers with feed through lugs

Product Line:
QO and Homeline load centers

Environment:
Product features

Cause:
Product availability

Resolution:

The Main breaker NEMA 1 load center with feed through lugs would be the QO12436M200TFT. 


CTA-ID : 2012284
Was this helpful?
What can we do to improve the information ?