Technical FAQs

Ask a Question

What is the magnitude and duration of the inrush for the NT shunt trip and closing coil?

The duration of the inrush current of the MX and XF coils is 200 VA or W during 200 ms.
Inrush A E
8.3 24
4.2 48
2.0 100
1.7 120
1.0 200
0.8 240
0.8 250


CTA-ID : 2012283
Was this helpful?
What can we do to improve the information ?