Technical FAQs

Ask a Question

What are the dimensions for the standard TVS unit EMA/EBA NEMA 1/3R/12 with no options?<br />With Integral Disconnect option?

No options = 14`` High, 12.44`` Wide, 6`` Deep
Integral Disconnect Option = 22`` High, 16.44`` Wide, 6`` Deep

CTA-ID : 2012271
Was this helpful?
What can we do to improve the information ?