Technical FAQs

Ask a Question

Is there a Dynamic Braking Transistor on the ATV58 HHP above 100 hp?

No. The Altivar58 drives from ATV58HC10N4 and larger do not include dynamic braking IGBTs.

A possible solution is to use an external braking module or regenerative unit, from another company to connect to the DC Bus. Consideration should be given to proper sizing and loading to avoid damage to the drive and dynamic braking components. SquareD can not take responsibility for any third party solutions.


CTA-ID : 2012902
Was this helpful?
What can we do to improve the information ?