Technical FAQs

Ask a Question

How do I change the LSP (Low Speed) in Altivar 28 drives?

Press the ESC key a few times then wait at least 3 seconds. The drive should be in the display mode.
Press ENT. This should display SEt.
Press ENT. At this point you are in the SEt menu.
Scroll down to LSP. Press ENT.
This will display the current value of the low speed parameter. The default value is 0.
Use the arrow keys to change the setting.
Press ENT. This will save the setting. The new setting is active.
Press ESC until you are at the display menu.

CTA-ID : 2012794
Was this helpful?
What can we do to improve the information ?