Technical FAQs

Ask a Question

Are the lugs in a PFA, PKA, PBLA and PTMA plug in unit replaceable in the field?

The lugs in the PFA, PKA, and PBLA plug-in units may be replaced in the field. Refer to the instructions that came with the plug-in unit or that came with the circuit breaker.

The PTMA lugs are not field replaceable.


CTA-ID : 2012730
Was this helpful?
What can we do to improve the information ?