Technical FAQs

Ask a Question

What is the plug-on extension kit for a QMB362T series D2 switch for mounting into the old QW(38-inch wide) interior?

Issue:
Product Design features

Product Line:
QMB Branch Safety Switches

Environment:
Plug-On Extensions

Cause:
application

Resolution:
The plug-on extension assembly required is the QMB306EX and this is ONLY For use in the Old Type QW (38-inch wide) Manufactured before 1984. 

 
Was this helpful?
What can we do to improve the information ?