Technical FAQs

Ask a Question

What is the Main bussing material used in the Catalog number EZM1800TB?

Issue:
Current design bussing material

Product Line:
EZM Metering

Environement:
Bussing material

Cause:
Application

Resolution:
The Main Bussing material used in the EZM1800TB is tin plated aluminum. 

CTA-ID : 2012725

has what looks like aluminum bus and the EZML112200 has what looks like copper bus.
Was this helpful?
What can we do to improve the information ?