Technical FAQs

Ask a Question

H328N dimension of the width of the enclosure is the same with or without the handle?

Yes, Handle is flange mounted on the front of the enclosure similiar to a combination starter?

CTA-ID : 2012718
Was this helpful?
What can we do to improve the information ?