Technical FAQs

Ask a Question

Is the VX4A66F1 a good part number for the control board for the ATV66?

This is a good part number if have an ATV66 Flux Vector unit.

The flux vector units use a different control basket from the standard units.

ATV66 FU41N4 to FD79N4 use VX4A66F1
ATV66 FC10N4 to FC19N4 use VX4A66F2


CTA-ID : 2012495
Was this helpful?
What can we do to improve the information ?