Technical FAQs

Ask a Question

Are the heatsink mounting screws provided with the FLEX 58 drive?

No the mounting screws are not provided with the FLEX converters. Figures 5 - 8 in the FLEX58 Chassis Drive Installation Guide (bulletin # 30072-450-47) provides the number, size and type of screw needed. The customer would be responsible for purchasing the hardware.

The instruction bulletin can be viewed by download from www.squared.com.


CTA-ID : 2012487
Was this helpful?
What can we do to improve the information ?