Technical FAQs

Ask a Question

Can we suppy 2000A or 3000A bus for HVL/cc connecting to Masterclad switchgear? This is for N3R Application.This could go in a PZ House or Sheltered aisle walk-in construction.

Issue:
Can we suppy 2000A or 3000A bus for HVL/cc connecting to Masterclad switchgear?  This is for N3R Application.This could go in a PZ House or Sheltered aisle walk-in construction.

Product Line:
MasterClad.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
NO. We cannot supply 2000A or 3000A bus for HVL/cc connecting to Masterclad switchgear. Use HVL switchgear.




CTA-ID : 2012486
Was this helpful?
What can we do to improve the information ?