Technical FAQs

Ask a Question

If load is removed from a transformer, with power on the primary, will the transformer be affected?

Transformers are not affected by the removal of the load.


CTA-ID : 2012892
Was this helpful?
What can we do to improve the information ?