Technical FAQs

Ask a Question

Does the HVL/cc have front access?

Issue:
Does the HVL/cc have front access?

Product Line:
HVL.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
Yes, the design of the 5&15kV HVL/cc is compact and front accessible. The larger 25kV-38kV HVL/cc requires rear access.


CTA-ID : 2012707
Was this helpful?
What can we do to improve the information ?