Technical FAQs

Ask a Question

What is the maximum HP of the 2510 KO1 at 115V single phase?

The maximum HP at 115 V single phase is 2 HP.


CTA-ID : 2012371
Was this helpful?
What can we do to improve the information ?