Technical FAQs

Ask a Question

Why won`t a job configure in the product selector when an incoming section for a Hot Sequence Meter Section is selected?

The reason that this job did not configure is that an incoming section was chosen for a Hot Sequence Meter Section. There is not a standard record to support this option.

Meter sections were designed for the incoming line to come in the rear of the enclosure.


CTA-ID : 2012483
Was this helpful?
What can we do to improve the information ?