Technical FAQs

Ask a Question

Can an additional cable be added to an HVL/cc switch with one cable per phase?

Yes, it is acceptable to add another cable into the field shaper on the HVL/cc switch. The HVL/cc will accept up to two 500 kcmil cables per phase.
A two-lug adapter must be ordered to allow two cables per phase.


CTA-ID : 2012481
Was this helpful?
What can we do to improve the information ?