Technical FAQs

Ask a Question

How many key locks can be installed on the HVL/cc switch?<br />Can they lock with secondary main breakers?

Two key locks maximum on the switch. (Small type)
Two key locks maximum on the ground switch. (Small type)
One standard key lock on the fuse panel.
Yes. We can interlock with the secondary main breaker.


CTA-ID : 2012480
Was this helpful?
What can we do to improve the information ?