Technical FAQs

Ask a Question

Can HVL/cc switches be accessed from the side?

Issue:
Can HVL/cc switches be accessed from the side?

Product Line:
HVL.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
HVL/cc switches can be accessed from the side only if there are end sheets that can be removed. The end sheets are only on the ends of a lineup. Single units would have 2 end sheets.


CTA-ID : 2012469
Was this helpful?
What can we do to improve the information ?