Technical FAQs

Ask a Question

What is the difference between an ATV58 TRX drive, and the standard ATV58?

The TRX is an upgraded version of the ATV58.  This upgrade was introduced with firmware version 5.1.  The biggest physical change is that an analog output was added to the Main Control board.  New parameters have also been added to the software, and can be accessed with a compatible keypad.

See the Keypad Display Programming Guide for ATV58 TRX AC Drives, VW3A58101. Firmware revision information is contained in this document.


CTA-ID : 2012510
Was this helpful?
What can we do to improve the information ?