Technical FAQs

Ask a Question

Can a dry type 600v or less transformer be installed indoors on a combustable material ?

Square D recommends low voltage dry type distribution transformers be installed according the installation instructions provided and in accordance will all applicable standards.

CTA-ID : 2012457
Was this helpful?
What can we do to improve the information ?