Technical FAQs

Ask a Question

What are the repair parts for a PAK41PGFI, Series E02, ServicePak Power Outlet Panel?

Only the parts listed below are considered field replaceable.
Panel Cover - 4054005101
Panel Cover Mounting Screw - (2) 2142717161
Pedestal Cover - 4054013801
Pedestal Cover Mounting Screw - (2) 4020513001K
Vapor Barrier Kit - 4028312851
Interior Trim - 4054008101
Interior Trim Mounting Screw - (2) 4020513001K
Interior Assembly - 4054019451 (Includes Base Assembly, Circuit Breaker(s) and Receptacle(s) shown below)
Base Assembly - 4054014050
Circuit Breaker - QO120GFI and QO130GFI
Receptacle - 4054001450 (125 volt/20 amp) and 4054004450 (125 volt/30 amp)
Receptacle Mounting Screw - 2190312160 (2 req`d for the 125 volt/20 amp receptacle)
Receptacle Mounting Spring Clip - 2330100001 (2 req`d for the 125 volt/20 amp receptacle)
Receptacle Mounting Screw - 2159412120 (3 req`d for the 125 volt/30 amp receptacle)
Loop Feed Phase/Neutral Lugs Assembly - 4054013550
Loop Feed Lugs Assembly Mounting Screw - (4) 2159417121
Loop Feed Ground Lug - (2) 4025104251, Mounting Screw - (2) 4020600903
Neutral Bonding Screw - Not Applicable
Ground Bar - 4023089855
Ground Bar Mounting Screw - 4020547901
NOTE: Covers and Interior Trims do not have labels applied.



CTA-ID : 14109
Was this helpful?
What can we do to improve the information ?