Technical FAQs

Ask a Question

What is the heater size for the Digest N3R Outdoor HVL Switches?<br /><br />Does the transition section to the PowerCast Transformer have a heater in it?<br /><br />Customer is trying to calculate the loading.

The heater size for the Digest N3R Outdoor HVL Switches is 1200 watts at 240V. To be operated at 120VAC producing 300 watts per section.

The transition section does not have a heater.


CTA-ID : 2012442
Was this helpful?
What can we do to improve the information ?