Technical FAQs

Ask a Question

Is there a 25kV 250E DIN/E fuse available for HVL/cc?

Issue:
Is there a 25kV 250E DIN/E fuse available for HVL/cc?

Product Line:
HVL.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
No. There is not a 25kV 250E DIN/E fuse available for HVL/cc?
The largest fuse size at 25kV is 180A which is a parallel combination of two 100E fuses.
Gaston will quote the NAL switch in Canada with boric acid fuses.
Our 25kV HVL switch is not UL or CUL.


CTA-ID : 2012440
Was this helpful?
What can we do to improve the information ?