Technical FAQs

Ask a Question

What are the standard number of spare auxiliary contacts for the Visi/Vac Circuit Interrupter?

The standard number of spare auxiliary contacts for the Visi/Vac Circuit Interrupter is 2 normally open and 3 normally closed.

2a and 3b contacts


CTA-ID : 2012433
Was this helpful?
What can we do to improve the information ?