Technical FAQs

Ask a Question

SG08168SG magnetic actuated sensor will not work using an ohmmeter as the load.

That is a triac output unit, which requires a 120V potential to operate. The ohmmeter battery will not turn it on. Put the sensor in series with a load at 120V (at less than 2A) to test it properly.

CTA-ID : 2012658
Was this helpful?
What can we do to improve the information ?