Technical FAQs

Ask a Question

Can the Altivar 58 open type H drive be ordered with the keypad included?

No. The keypad must be ordered separately. The keypad part number is VW3A58101U.

At the top of page 118 in the Altivar 58 AC Drives catalog (8806CT9901 dated August 200) is shows that ATV58 drives can be ordered to included the keypad if the last numbers are changed to KU instead of ZU. This note is not correct.


CTA-ID : 2012656
Was this helpful?
What can we do to improve the information ?