Technical FAQs

Ask a Question

Can zone interlocking be done with both 100% full function, & 80% standard function breakers??

The Zone interlocking function can only be obtained using the 100% rated full function ie( LE, ME, PE, NE, SE) breakers. It is not available using the 80% (LX, MX, NX, PX) breakers

CTA-ID : 2012654
Was this helpful?
What can we do to improve the information ?