Technical FAQs

Ask a Question

Which is the neutral pole on a 4-pole NW?

The neutral is the left pole. It is protected, and a neutral current transformer NCT is not required if sensing ground-fault.


CTA-ID : 2012406
Was this helpful?
What can we do to improve the information ?