Technical FAQs

Ask a Question

How can the logic output be connected to be used as an analog output?

When using the logic output to represent an analog value for a PLC input or a meter, the drive actually uses a 15 VDC pulse width modulated (PWM) output to simulate an analog signal. This signal must be conditioned with an RC circuit into an analog signal such as 0-5, 0-10 VDC or 0-20 mA based on the impedance of the receiving device.
NOTE: The link contains a document that is not for general distribution.
For details, contact Drive Products Support at 888-SQUARED or E-mail drive.products.support@us.schneider-electric.com


CTA-ID : 2012404
Was this helpful?
What can we do to improve the information ?