Technical FAQs

Ask a Question

How does an HP3F hanger mount to an AP504-G10 bus? Contractor claims it is too loose.

The hanger is installed by placing the hanger lengthwise to the bus and into the opening on top of the busway. Twist the hanger so that the bus housing fits into the hanger slots. The hanger is hung from a threaded rod, provided by the installer, which fits through a hole in the top of the hanger. A tight fit is not to be expected. See picture in installation instructions or in the Busway Systems Class 5600 manual.


CTA-ID : 2012401
Was this helpful?
What can we do to improve the information ?