Technical FAQs

Ask a Question

What is required for factory installation of a High-Low selector switch for the Class 8810 reversing type two speed starter?<br /><br /><br /><br />

Use factory modification Form C17 for High-Low and use Form C14 for Forward-Off-Reverse.

CTA-ID : 2012848
Was this helpful?
What can we do to improve the information ?