Technical FAQs

Ask a Question

What other depths of HVL switchgear are available at no charge?<br />

46.50`` and 36.00`` depths are available at no charge, but not selectable in the product selector. These depths must be tagged in. Layouts may be required. The Product Selector configuration logic supports only 54.50`` layouts. These reduced depths limit what can be installed in the sections.

CTA-ID : 2012625
Was this helpful?
What can we do to improve the information ?