Technical FAQs

Ask a Question

Why was an HVL duplex switch was entered in the Product Selector shown as 78`` deep. The standard depth is 54.50``.<br /><br />What can be done to reduce the depth to 54.50``?<br /><br />

The duplex switch enclosure must be made 78`` deep if there is top or bottom entry with large cables or several cables per phase.

Top entry can be possibly be helped by adding a pullbox on top.

CTA-ID : 2012623
Was this helpful?
What can we do to improve the information ?