Technical FAQs

Ask a Question

What causes base undercoating to be ``locked in`` in the product selector?

On outdoor N3R enclosures, if bottom plates are selected, then base undercoating is required. There is a reduction of air flow through the base and undercoating protects against trapped moisture.



CTA-ID : 2012620
Was this helpful?
What can we do to improve the information ?